DLPA100: The minimum color segment degrees which DLPC3440 and DLPA100 can support

Part Number: DLPA100
Hi TI,
I have a question about a color wheel design. 
My optical design team is going to decide each segment degrees of a color wheel R, G, B for the next design and they are wondering what is the minimum degrees which DLPC3440 and DLPA100 can support? 
According to the datasheet of DLPC3440, 14%(50.4deg) is described as the minimum degrees in the case of 180Hz CW speed in figure 25 page 44. 
What if it is 120Hz CW speed? 
It would be helpful for me if you could let me know. 
Best regards, 
Hide