Other Parts Discussed in Thread: DLP3010, , DLPA2005
I am using the DLPC3433 with DLPA2005 and DLP3010.
I currently do not have the DMD connected but the DLPC and DLPA are set up.
I flashed the firmware from TI using flashrom and raspberry pi.
I turn PROJ_ON high
- RESETZ goes high
- Power rails go to ~5V
HOST_IRQ stays high which means the DLPC hasn't finished initializing.
Questions:
Does the DMD need to be connected for the initializing of DLPC to finish?
Does this indicate that the firmware was not correctly flashed?