DLP2000: External rotating filter with motor for DLP2000EVM (DLPC2607) instead of 3 color LEDs?

Part Number: DLP2000
Other Parts Discussed in Thread: DLPC2607, DLPDLCR2000EVM

Hello!


Is it possible to use an external motorized rotating filter for DLP2000EVM instead of 3 color LEDs?
How to synchronize a micromirror DLP2000EVM (DLPC2607) with an external rotating light filter from the engine?
In what time interval is it possible to switch micromirrors:
- for a 3 color filter with a motor?
- for a 2 color filter with a motor?

Respectfully yours, Vladimir Zhukov.

  • Zhukov,

    The DLPDLCR2000EVM only supports 3-color LEDs for illumination. A filter with this sort of illumination setup is not supported. In particular, the illumination time intervals are not user-controllable for this chipset.

    If you want to be able to customize the illumination exposure period for the color channels you will need to use one of our Light Control chipsets to do this (such as the DLPC347x).

    Best Regards,

    Philippe Dollo