Other Parts Discussed in Thread: DLPC3470, DLP2010,
Greetings,
I am using the DLPA2005 + DLPC3470 + DLP2010 chipset, and enconter a problem.
When the PROJ_ON goes high, the system power-up and after about 400ms(VRST, VBIAS, VOFS are on)
the INTZ on DLPA2005 gose low and the DMD is turned off.
The DLPA2005 is powered by 3.3V voltage support, insted of 5V on EVM.
Is there any thing to do with this change?
Thank you!