This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DLP3010EVM-LC: Write Flash Start Command

Guru 12300 points

Replies: 6

Views: 289

Part Number: DLP3010EVM-LC

Hi,

Let me talk about DLP3010EVM-LC.

The following commands are executed when write a 1 or 8 bit image to flash with TI's tool.
The first 64 bytes look like header data, followed by image data.

EX)
Write Flash Start:
E1         [command]
50 41 54 4E 48 00 ... [64byte]
00 00 34 00 00 00 ... [data]


What is this 64byte ?
I see section 3.7.6 of DLPC3470 and DLPC3478 Software Programmer's Guide.

But I can not find this description.

Best Regards
Hiroyasu

  • Hi Hiroyasu,

    Kindly wait for sometime and someone from our team will look into this shortly.
    Thanks & Regards,
    Hirak.
  • Expert 5485 points
    Hi Hiroyasu,

    Can you explain when these commands are executed? What action in the GUI led to these commands being executed?

    Regards
    Azad
  • In reply to Azad:

    Dear Azad

    It is executed when We click "Program & Load Pattern Data".

    Best Regards
    Hiroyasu

  • Expert 5485 points

    In reply to Hiroyasu:

    Hi Hiroyasu,

    Thanks for the clarification.

    As you mentioned the first few bytes consists of the pattern block header and the pattern set header.

    We are developing sample code which will allow users to generate their own pattern data without using the DLPDLC-GUI. This sample code will explain the structure of the pattern data block and how to generate it. This will be released on ti.com in a few weeks. Request you to please wait for this release.

    Thank you for your patience.

    Regards
    Azad
  • In reply to Azad:

    Dear Azad

    Thank you for your reply.
    I understood. Could you tell me after you complete ? 
    and We want more discription of this command.

    Thank you !

    Best Regards
    Hiroyasu

  • In reply to Hiroyasu:

    Dear Azad

    We want description for detail of header before you complete if you are possible.

    Best Regards
    Hiroyasu

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.