Hello,
I am working with a 0.7 XGA 2xLVDS Type-A DMD for beam-shaping purpose in a cold atom physics experiment. The wavelengths I work with are near or above 800 nm.
The informations on maximal light input power I found on www.ti.com/lit/ds/symlink/dlp7000.pdf are : 25 W/cm^2 between 400 and 700 nm, 2 mW/cm^2 for wavelengths under 400 nm and 10 mW/cm^2 for wavelengths above 700 nm.
These values with a very big drop for non visible wavelength seem very strange, and it is very difficult to get an idea of the evolution of the DMD absorption with respect to the wavelength with only three data points.
- Do you confirm the values written above?
- If so, what is the element causing so much absorption above 700 nm?
- In what material are the mirrors made?
- Could you please provide a graph of the evolution of the DMD absorption with respect to the wavelength?
- If this graph doesn't exist, could you at least provide the theoretical absorption of the DMD around 800 nm?
I thank you in advance for your response.
Best regards,
Guillaume Coppola
Laboratoire Kastler Brossel