In the LightCommander 9000 EVM, will the DLPC900 controller allow me to to hold the DMD in a fixed pattern (that is, without returning mirrors to the flat/reset position)? We want to be able to dynamically generate monochromatic (black and white) patterns from a computer and have the DMD hold this pattern until the next one is set.
It seems like this would be impossible in video mode since the controller automatically cycles between the red, green, and blue colors. From my understanding, all of the mirrors would be brought back to the flat/reset position between each color, even if the red, green, and blue patterns were identical. And, it would also reset every mirror back to the flat position between every video frame. Is my understanding correct?
If so, would it be possible to do this with pattern-on-the-fly mode instead? Section 4.2.3.4 of the DLPC900 Programmer's Guide seems to indicate that we can have 1-bit bit-depth patterns, but Section 4.2.4 specifies 24-bit BMP images (which I assume are color images). Can I use pattern-on-the-fly mode without automatically cycling between red, green, and blue?
Also, how long can I safely leave the DMD mirrors in a fixed position? The DLPC900 Programmer's Guide and some of the other documentation seems to indicate that leaving the mirrors in their on or off state for a long time will cause damage and suggests either parking the mirrors in the flat/reset position or enabling "Idle Mode" as often as possible.
Thanks in advance,
-Jimmy