Hi,
Planning to use the LightCrafter 9000 with a laser source, I would like to generate 1bit patterns with rates > 1 KHz.
First, I've seen different Max Rate informations in the documentation :
- DLPU018B, table 2-79, we have 120 Hz for WQXGA
- DLPU028B, table 3-1, we have 60 Hz in for WQXGA
From my understanding, the only possibility with the EVM :
DP @60Hz, 24bits -> 24*60=1440 Hz or 2880 (depending on the 60 or 120 Hz compatible refresh rate of my first question)
But i didn't get how can I decompose the 1x24 bit video input in 24x1bit output patterns yet.
Is it possible to use the DLP LightCrafter 6500 & 9000 GUI tool, using the pattern mode, for video pattern mode, to split the 24 bit frame in 24 1bit pattern ?
Thanks in advance for your support.
Regards