This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 2841
Hello,
For the 0.95" 1080p, I was wondering what is the exact dimention of a single micromirror and the gap width between the mirrors? Another thing I'd like to know is the shape and the size of the "Via" at the mirror's center. Is the Via square and rotated by 45 deg with respect to the micromirror? How much of light loss at the Via compared to the gap? Does the fill factor of ~92.5% include the Via?
A paper on the net (http://arxiv.org/PS_cache/arxiv/pdf/0804/0804.4433v1.pdf) described the gap width was 0.6 um, but I was not sure if it's correct. I thought it should be approximately 0.41 um based on the mirror pitch of 10.8 um and the fill factor of 92.5%.
I would be very appreciate it if you could let me know those dimensions.
Thank you in advance.
J. Jang
J. Jang,
Thank you for your inquiry.
The 92.5% fill factor is accurate on a standard DLP projector illuminating at a 24 degree angle of incidence. This fill factor includes the mirror via.
Unfortunately I can not give you the exact dimensions or shape of the mirror via because that is TI Proprietary information.