This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC910: Any sample code of the Apps FPGA for DLPC910 available?

Part Number: DLPC910
Other Parts Discussed in Thread: TIDA-00570, , DLPC410

Dear All,

Please let me ask you the availability of the sample Apps FPGA code for DLPC910 chip-set reference design(TIDA-00570).

If my understanding correct , I noticed there is no sample code.

Is there the plan for the code release?

Best regards,

Rossinag

  • How good to hear from you again Rossinag-san,

    Currently there is no plan to provide sample code for the APPS_FPGA connected to the DLPC910 in the reference design.

    However, since the APPS_FPGA code for the Discovery 4100 kit (DLPC410) is very similar, it should be able to be modified without too much effort.  You would have to change the LVDS clock speed and the length of the row SERDES buffers to match the row load length and the pattern_generator to put out 40 bits per row cycle (i.e. 20 clock cycle row length).

    Fizix