Part Number: DLP2010EVM-LC
dear Sir.,
where is the save pattern data and how can I use the save pattern data?
2. from ticket below.
https://e2e.ti.com/support/dlp/f/94/t/729968
There is max # of patterns for 1D pattern type.
-
1D Pattern Type Max # of Patterns 8-bits vertical patterns 6 8-bits horizontal patterns 8 1-bits vertical patterns 51 1-bits horizontal patterns 64 627334b3-49ce-4ac7-83b3-3ba90b7da7b5.logCrash File for DLP Pico Display and Light Control EVM 1.1.0.7 (Build 20180913, #1efecf6) Current Time: 10/4/2018 4:09:29 PM Message: 10/4/2018 4:09:29 PM Exception : Specified argument was out of the range of valid values. Source : DLPComposer.XUI.Data TargetSite : T get_Item(Int32) Stack Trace : at DLPComposer.XUI.Data.ComplexElementClassList`1.get_Item(Int32 Index) at DLPComposer.LightCrafter.UI.LightControl.PatternControlPage.ValidateInternalPatternSettings() at DLPComposer.LightCrafter.UI.LightControl.PatternControlPage.btnProgramDataToFlash_Click(Object sender, EventArgs e) at System.Windows.Forms.Control.OnClick(EventArgs e) at System.Windows.Forms.Button.OnClick(EventArgs e) at DLPComposer.LightCrafter.UI.Controls.FlatButton.OnClick(EventArgs e) at System.Windows.Forms.Button.OnMouseUp(MouseEventArgs mevent) at System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks) at System.Windows.Forms.Control.WndProc(Message& m) at System.Windows.Forms.ButtonBase.WndProc(Message& m) at System.Windows.Forms.Button.WndProc(Message& m) at System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m) at System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m) at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam) Data : InnerException : null
It means that if the pattern data is over the table above, the DLPC would reload the 1D pattern from flash. Customer needs to check the pattern ready pin for following pattern, right?
at this condition, the speed for 1D\ 1bits pattern would not be 2.5KHz. Any information about the pattern ready pin would be ready
by the way, when i increase the pattern set to 4 sets, the program shows an error as attachment.
BR,
frank