Other Parts Discussed in Thread: DLP660TE,
Hi TI
hardware platform:4K UHD High Brightness Display Reference Design using TI DLP® Technology
http://www.ti.com/product/DLPC4422/toolssoftware
Firmware version :DLP660TE_Chipset_Firmware_v8.1 , Download from http://www.ti.com/lit/zip/tidcd51a
Functions currently implemented:
1、DLPC4422 GUI 1.0 + USB + Device = OK ,Set and Get
Problems currently encountered
1、DLPC4422 GUI 1.0 + DeVaSys + Device = ERROR ,Set or Get
2、DeVaSys device connect UHD PCB board J10 \ J12 \ J13, but The results are the same., ERROR !!!
3、I can confirm. DeVaSys device is OK, EDID can be Programed by it
4、 iic0 iic1 iic2 , I suspect they all work in the slave mode.
1、DLPC4422 Software Programmer's Guide,There is no explanation for using which IIC interface
I assume that version 8.1 firmware does not support IIC slave control
Now,The function I need to implement is to control DLPC4422 through IIC interface of STM32 controller.
Please TI to determine whether firmware is a problem
Thanks