This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP7000UV: DLP7000UV

Part Number: DLP7000UV

Can this (or another product) be used at a wavelength of 355nm?

Thanking you,

Shanti

  • Hi Shanti,

    You can use it but its not characterised below 363nm. You need to make sure operating conditions e.g Illumination power density, temperature etc are followed for < 363nm as explained in Section 7.4, Section 8.6.3 and Section 9.2.5 of datasheet.

    -ykc