Other Parts Discussed in Thread: DLPDLCR2010EVM-PCB, DLPC3435
Hi All :
We bought some DLPDLCR2010EVM-PCB for develop, we want to create the image to set crop image resolution(854*480), change duty circle and current on the look 1, look 1 is the default look when we open the projector.
We following the steps like below : Using Light Crafter Display v7.0 software
1. We use the software to backup the projector image. When we open the projector we can see the crop resolution is 1280*800(this resolution maybe is EDID?) and the default look is look 1.
2.Using DLPC3435_3.0.0_Firmware.im_.img as the base to change duty circle and current and create the image.
3.Using software to update the image which we create to the projector.
After these steps, we can see the crop image resolution is 520*320 and the look 1 isn't our set duty circle, we found the correct duty circle is in the look 3 when we open the projector.
How can we update the image to change current and duty in the default look 1 and don't change the crop image resolution?
We want to open the projector and see the crop image is 854*480 and correct current and duty in the default look.
Please help us to resolve this issue.
Thanks.