This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPD4X00KIT: DLPD4X00KIT and DLPLCRC410EVM - what do i need to load a custom code on the fpga ?

Part Number: DLPD4X00KIT

Hello 

I just bought a DLPLCRC410EVM and a DLPLCR70EVM.

In the next future i'll try to develop a custom FPGA code (starting from the D4100APPSPGEN-2.0 one)  in order to understand how the input to DLPC410 is supposed to work.

Such FPGA code is supposed to run on the ApplicationsFPGA (APPSFPGA)

What do i need to program the FPGA?

  • About the hardware i need a programming cable such as HW-USB-II-G made by xilinx ( should be the replacement of the old DLC9G )  - is it correct ? 
  • About the software: what do you guys suggest ? I need both to load the code on the FPGA as well as i need to simulate it

Also, the source VHDL code in D4100APPSPGEN-2.0, how am i supposed to compile it ?  

Thanks 

Federico