Other Parts Discussed in Thread: DLPA2005,
Hi All,
I am bringing up a projector board that uses the DLPA2005 and DLPC3470. I was having an issue with the crystal oscillator, but that turned out to be a defective board since the second board's oscillator is running fine.
Now I believe the 3470 is trying to boot but not getting the appropriate data from Flash. I don't see the 3470 sending a read command to Flash since the DI signal is always low. The Flash ROM, W25Q32 (133 MHz) have been pre-programmed with code Kyle sent me (ASIC routing option 4).
Can you tell me the details of the boot process and what happens in the event of errors?
Below I've shown the key Flash signals: CS, DO and CLK. As I said above, DI is always low. All the traces are 50us/cm.
Thanks,
Scott