Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLP4710EVM-LC, DLPDLCR4710EVM-G2
I posted this as a follow-up question on another recent thread, but it's really a separate question. Since I didn't get a reply, I'm posting it in a separate thread.
I want to use the 3010 or 4710 as high-frequency monochrome projectors, driven by a GPU over HDMI. I would settle for 1440 Hz output at 1 bit, but anything higher would be better.
1. The 3010 has a mode with 200 µs - 399 µs exposure time and 202 µs of pre- and post-exposure total dark time. At 200 µs exposure time, that works out to about 2488 Hz output frequency, and -- assuming you squeeze the 24 images into the 24 RGB bit planes -- 103.6 Hz input frequency. I assume that a 103.6 Hz output over HDMI isn't achievable. If we want an integer input frequency, we can try for 103 Hz, which would correspond to an output frequency of 2472 Hz and an image duration of 202.5 µs; or if we like round numbers, then we could try for 100 Hz input frequency, which would give an output frequency of 2400 Hz and an image duration of 214.7 µs.
Are these assumptions correct -- is that how you would have to drive the 3010 EVM to get the highest possible 1-bit output frequencies, by varying the input frequency of the HDMI signal? If so, do you know if that's achievable using GPUs over HDMI outputs? The Wikipedia article on HDMI states that versions 1.0 and 1.1 of HDMI were restricted to certain refresh rates, like 60 Hz, but starting with version 1.2 arbitrary refresh rates became possible. Have you or any of your customers been able to achieve these high refresh rates using HDMI output from GPUs at refresh rates like 100 or 103 Hz?
2. The 4710 can output at 1440 Hz at 1 bit depth in external streaming mode, right? If so, can I drive it using a 60 Hz signal from a GPU, squeezing 24 frames into the 24 bit planes of each frame?
3. Question about the different colored LEDs: in the 2488 Hz mode of the 3010, or the 1440 Hz mode of the 4710, can one have the 3 LEDs turned on simultaneously to get true white (rather than cycling through the red, green and blue LEDs through successive frames)?
Thank you very much for your help.
Mark Wexler