hi
need to purchase ready to use optical module for DLP 4710 with uv 405 nm led based projector
the list of vendors from china available on ti.com are contacted but not responding on email.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
need to purchase ready to use optical module for DLP 4710 with uv 405 nm led based projector
the list of vendors from china available on ti.com are contacted but not responding on email.
Hi Pratik,
We have ready optical module of DLP4710 Projector mainly for 3D printing.
If you are Interested , please send me e-mail: chenhf@dspchina.com
Here is the specifications:
Items |
Specification |
Mark |
Light Source |
UV LED |
|
Uniformity |
>95% |
Uniformed by the lenslet array |
Output power |
>600mw |
|
Micro-mirror pitch |
5.4um |
1080P |
Thermal |
Air Cooling |
|
Lens working distance |
114mm |
Available for custom made.
|
FOV |
96mm*54mm |
|
Unit Size |
217mm*82mm*68mm |
|
Weight |
Around 1kg |
|
Prateek,
Please contact the engine provider at the mentioned email address.
regards,
Vivek.