This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: Disable or change splash screen possible?

Part Number: DLPDLCR2000EVM
Other Parts Discussed in Thread: DLPC2607

Hello,

I have a working setup with a Pi Zero.

A small python-script waits for a falling signal on one of the Pi GPIO pins.

If this happens, i activate the EVM with "PROJ_ON_EXT" = high

After that i start a videoplayer (omxplayer).

It works fine so far... But the omxplayer needs a fews seconds to start and for this time, the splash screen of the EVM appears.

My Question is:

Is it possible to disable the splash screen, or to change it to complete black?

regards

Reiner