I would like to know a mechanism for programing&loading 1D patterns.
In GUI, Light Control > Internal Patterns > Pattern Set Order > 4. Program the Flash.
Regarding #4 process, is my below understanding correct?
1. The patterns as #3 process(Define pattern set display order and configuration) are written to a flash via Cypress-SPI.
2.The command as "98h:Write Pattern Order Table Entry" is sent to DLPC via Cypress-I2C.
3. The patterns saved in flash are loaded to DLPC RAM.