This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR9000EVM: External trigger

Part Number: DLPLCR9000EVM

Hello.

I tried to put external trigger into my DMD, but failed. 

I am using 51021-0600 for connector and 50079-8100 for crimp. 

I put a rectangular wave which is 1kHz, and 3.3V, but it didn't work. 

So I checked whether trigger out was working well or not. 

Checked by the oscilloscope, it also didn't work. 

It can be a connector problem? If not, what should I do then?

Thanks.