Hi,
I have defined my own connectors and cabling between my two board designs. One board is the DLP controller board using two DLPC900s, and the other is the micromirror board using the DLP9000. I have both schematics from the DLP9000 Lightcrafter EVM reference design, and the signal names between the two schematics are different. The mapping from one connector to the other, with the Amphenol cable(s), is confusing to me. I have determined the following matching:
DLP side | DMD side |
DADOEZ | DAD_OEZ |
DADINTZ | DADIRQZ |
SSP0_RXD_S2M | SCP_DO |
SSP0_CSZ1_DMD | SCP_DMD_CSZ |
SSP0_CSZ0_DAD1 | <UNUSED> |
SSP0_CXZ5_DAD2 | <UNUSED> |
SSP0_TXD_M2S | SCP_DI |
SSP0_CLK | SCP_CLK |
DADSTRB | DADSTRB |
DADADDRx | DAD_ADDRx |
DADMODEx | DADMODE_x |
DADSELx | DADSEL_x |
M_EXT_RSTZ | DMDRSTZ |
I would like someone to confirm that I got this right.
Thank you,
Hanson