Hello,
First of all thanks to Hirak who helped me a lot to get my Nirscan Nano running under C#. Meanwhile the software works fine.
1. My next task is to reduce the measurement time. First tests showed that I have to average at least 3 scans to get a reliable result. I switch on the lamps pemanently to reduce the warm up time. Now the estimated scan time is 0.75 s, the actual scan time is about 1.0 s. Do you know why the two values differ? I would lime to reach about 0.6s. Are there any more possibilities to reduce the measurement time? As far as I know, the number of scans can be reduced, the lamps can be left on permanetly and the prescan can be omitted. Do you have any more ideas?
2. I have to integrate the device into an existing process. As the space is limited, I should place the sensor in a certain distance to the measuring position. I think I should use an optical fibre to reach the measuring position. Could you recommend a product or a manufacturer of such a fibre which is propriate for the Nirscan?
Thanks & Regards,
Simon