Other Parts Discussed in Thread: DLPLCRC410EVM
Hello,
I design a board with the DLPC410 which controls DMD at data rate of 800Mbps.
My question is regarding the DLPC410 Ref Clock: "CLKIN_R".
According the datasheet - "The reference clock, CLKIN_R, supplied from an oscillator must be 50 MHz".
However I couldn't find any constraints/requirements on the clock signal except of voltage levels of the LVCMOS2.5V, furthermore - in the EVB reference the clock is sourced by an FPGA I/O .
Can I use FPGA's I/O as a clock source with no concerns or should I use a dedicated oscillator ?
Thank you very much.
Ohad