Hi
We have been experimenting with the 4710-LC EVM and just finished
setting it to sync with our sensor. The result is pretty
good, however our depth of focus is limited and we seem
to have too much background noise that is too noticeable
especially when using our smallest light features pattern,
as if there is a leak of light or the black is not fully black.
we realize that the contrast is a bit low and therefore we work
at lower power, however we would like to work at higher intensity level especially when using it
on our targeted materials which absorb more light, yet avoid too much surrounding noise which becomes
apparent when we use it on other surfaces. is there other projection optics that
can offer better depth of focus and low noise?
Our operating distance vary from 45cm to 80cm.
thanks