Part Number: DLPLCR6500EVM
Hi,
I am using the 6500EVM in a sinple-pixel imaging application. In my experiment, illumination lights are irradiated to the DMD and all the lights reflected on the "on-state" micromirrors are collected with lenses and detected with a fast single-pixel detector. The 6500EVM is operated in "Pattern on-the-fly" mode with 400 images. I found spike-shape noises every 105 μs in the time domain like the image below, even though I set the exposure time of the 6500EVM to much larger time period like 3000μs. I would like to avoid that noises because they will strongly distort outputs in our experiment. What is the possible cause of it, and is there any way to avoid those 105μs noises when the exposure time is set at larger time period than 105 μs?
I have seen similar periodic noises when I used a DLP rightcrafter in the "static image" mode, but they disappeared when it is operated in the "internal stored pattern sequence" mode. therefore, I hope there is a way for the 6500EVM as with the DLP rightcrafter.
In addition to it, I would like to synchronize the 6500EVM with external trigger generated with a functional generator. If there is a solution to the problem, is it compatible with controlling DMD with external triggers?
Thanks.
(The intensity is recorded with a AC mode detector)