Part Number: DLP5531-Q1
Other Parts Discussed in Thread: DLP5530Q1EVM, DLP5531Q1EVM
Hello Jake,
with reference to the difference between DLP-553X-Q1 models mentioned above, I take this opportunity to ask you which model you recommend to develop high brightness FULL COLOR laser projector using sequentially activated laser beams (RGB).
From the functional diagram of DLP5531-Q1 & DLP5534-Q1, both seem to work with 1 control light source (without the possibility of using it for the color application), while instead the DLP5530-Q1 model has separately the control of 3 light sources (RGB - LED / Laser).
Is it correct?
We plan to use an RGB laser source with a power up to 10 W (total RGB power).
Please let me know the correct DMD choice and the electronic evaluation you recommend.
Many thanks in advance.
Kind Regards,
Gian Paolo