Hi, I am working with a DLP6500 in an application where I am using the pattern on the fly mode, and loading images to the board. I have a custom test GUI that I use to load images by calling a driver that sends USB HID commands to the board. With firmware version 4.x, I am able to successfully load images, however when I move to firmware version 5 I am no longer able to successfully load images. Note nothing is changing in my software, it is purely a firmware change on the board. I am still able to load images through the TI example GUI for either firmware version.
Is there anything in the protocol to the board that has changed for version 5? Were any bugs fixed such that if my driver was sending a message that wasn't 100% correct it would previously work, but will no longer work?
Thanks,
Paul