This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3438: DPLC does not start, HOST_IRQ stays high

Part Number: DLPC3438
Other Parts Discussed in Thread: DLP3010, , DLPA3000, DLPDLCR3010EVM-G2

I have got a PCB where I want to use a DLPC3438 with an DLPA3000 and a DLP3010. The HOST_IRQ does not go low.

The firmware I use is from the DLPDLCR3010EVM-G2. Version 7.3.3

We have checked the System Power-Up and Power-Down Sequence:

* Voltage Levels (1.1V, 1.8V and 3.3V) from the DLPA are good and noise is within tolerance.

* After PROJ_ON is high PARKZ is on 1.8V

* PLL_REFCLK is a stable 24MHz.

* HOST_IRQ goes high

* RESETZ goes to a high Level

* There is no activity on the I2C Bus

* I can see data on the SPI-Flash interface for a while and it then stops.

* I can see data on the SPI Interface to the DLPA for a bit and it stops.

* There is no clocking on the DMD_LS lines.

* HOST_IRQ stays high!!

* No communication on the I2C with the DLPC is possible.

We have verified the content of the Flash chip, it matches the dpp343x_7.3.3.img

Do you have any suggestions where we can check why it is not starting?