I had a couple questions regarding I2C communication with the 2000EVM. In the programmer's guide it says that the EVM is rated up to speed of 400kHz. My current PIC has problems with speeds at 400kHz so I have moved it down to 100kHz with 2 10K pull up resistors. Will that work with the EVM?
Also, I am initially just trying to get the splash screen to change. So far I've sent:
0x36 0x0b 0x00 0x00 0x00 0x01 (sub address for input source selection - set to internal test pattern)
0x36 0x0c 0x00 0x00 0x00 0x1b (sub address for input/output resolution - set to nHd landscape)
I noticed that in the quick start tutorial they set the address of the evm to 0x1b. I assume that is specific only to communicating with the beaglebone. I have a beaglebone and tested the evm with that and everything works perfectly. Just need to get it working with the PIC now.
Thanks.
Lance