Other Parts Discussed in Thread: DLP4710
Hello,
just want to ensure that our understanding of datasheet is correct. We think of using DLP4500 in low temperatures (could be as low as 0°C). Datasheet specifies the low end of operational temperature as 0°C, while "DMD temperature - operational, long-term " is specified from 10°C, but if understood the note well, it is an average temperature over the life time? Therefore powering and some initial operation of DMD at 0°C should be OK, as far as in average the DMD is kept at or over 10°C, and there will not be any impact on the DMD lifetime?
Thanks
Petr