About DLP2010NIR & DLPC150,we needs to scan all columns each in 1 sec for optical perfotmance monitoring in DWDM system. How to do?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About DLP2010NIR & DLPC150,we needs to scan all columns each in 1 sec for optical perfotmance monitoring in DWDM system. How to do?
Hello ,
Welcome to DLP forum and thank you for your interest in DLP technology.
What is optical wavelength used in your application?. The DLP2010NIR DMD is designed for wavelength from 700 nm to 2500nm. The DLP2010 DMD is for visible range. Please select the appropriate DMD based on your application.
DLPC150 controller will work with both DMDs. It can also support the required scan rate for your application. I understand that you would like scan only one column of mirrors at a time and scan complete DMD (854 column) in 1 second.
Please refer to DLPC150 programmer guide for details of the command and configuration.
https://www.ti.com/lit/ug/dlpu031a/dlpu031a.pdf?ts=1588112046906
You can pack patterns in to a 16-bit (RGB565 ) format or 24-bit (RGB888) format image. The complete pattern set (864) could be sent over in 54 frame (for 16 bit format) or 36 frames (24 bit format) over parallel port interface.
regards,
Vivek