Part Number: DLPLCR9000EVM
Hello,
I believe there is an error in my DMD board.
In the lightcrafter GUI, I get a DMD incompatible error. I searched the E2E threads and it seems to be a common error.
I check the testpoint voltages and compared the following:
Voltage | Nominal Value | TestPoint |
---|---|---|
VCC | 3.3V | J3.1 |
VCCI | 3.3V | J3.1 |
VOFFSET | 8.5V |
TP4 |
VBIAS | 16V | TP6 |
VRESET | -10V | TP5 |
Here are my values:
J3.1: 3.3V
TP4: 3.1V (should be 8.5V)
TP6: 330mV (should be 16V
TP5: 360 mV (should be -10V)
Note that this was not done with "J1" shorted which might be needed to enable U1. I could not find a way to short J1.
From previous threads, if TP4, 5, and 6 are off, the culprit could be L1 or U1.
If this is the case, Can you suggest a part number for L1? All I could find was that the resistance should be like 220 Ohms at 100MHz. Any suggestions on specific replacements?
Thanks!
Kevin