Part Number: DLPDLCR2010EVM
Hi Team,
We received an inquiry from a customer and we would like to consult his concerns with you. Here are the details of his inquiry.
I would like to use a DLP chip to produce directed beams/rays of light. In the application the light angel is from importance, and beams/rays with different directions must be produced.
The question is, is the DLP switching characteristic exact enough to calculate the reflection angel of one micro mirror during its switching cycle, or can a DLP chip only be used as a binary direction changer, with no intermediate locations.
im aware there exists at least some chips with more then two discret positions, for virtual 4K image creation. They can shift to pixel_position_1, pixel_position_2 and off_position.
do chips exist with more discret positions?
Regards,
Danilo