I am looking at the white paper saying a maximum power of 25W/cm^2 can be applied for DMD chip. But for pulsed laser, it may be different becasue of high peak power. So I have the following questions:
1. For 10fs~100fs, 800nm laser with rep rate of 1MHz, is the heating effect almost the same as the continous laser with the same average power?
2. Does the array temperature changes according to different laser specs?
3. Finally, I want to know if 25W/cm^2 is a safe number that I can apply with the laser specs I mentioned in 1.
Thank you!