This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DLP9000: Real time pattern reading

Prodigy 30 points

Replies: 2

Views: 72

Part Number: DLP9000

Using the TI software, we can only preload the patterns into the flash and then display them. Is it possible to load the patterns in real time?

For example, I select a folder from the computer and then start the DMD. Then the DMD will automatically read one image, display it and then read another image, display it...Till it reads and dispalys all the images in the folder.

Thanks!

  • Hello Cheng,

    I am a little confused.  Is this the DLPC900 controller (with DLP9000) or the DLPC910 controller (with DLP9000X)?

    I ask because with the DLPC900 you can load up to 400 1-bit or up to 50 8-bit patterns directly to controller memory and display them.

    With the DLPC910 controller if you are using the GUI it can only load one image at a time from the GUI.

    Fizix

  • In reply to Fizix:

    Cheng,

    Did you still need assistance with this question?

    Fizix

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.