Hello everyone,
I found the design of a fiber connection module for the NIRscan Nano on your homepage and I am currently trying to build it myself since Optecks and TI do not sell it anymore to my knowledge.
I asked the questions below already to Optecks and they told me to write to TI directly.
I have some questions about the fiber that should be used for this connection module:
For maximal signal a round to linear fiber should be connected to the spectrometer to illuminate as much of the slit area as possible.
I assume the design was done with a Thorlabs-fiber bundle in mind, since the SMA-connector is also a Thorlabs-part.
I wanted to ask what fiber diameter is best to use ?
Thorlabs offers two options namely 105µm and 200µm, which one is best suited for the module ?
Thanks in advance and best regards,
Robert