Other Parts Discussed in Thread: DLPA3005, TPS54335A
Hello TI team,
I have got a question about the input power for DLP4710EVM-LC.
It is written In the user guide that a DC power supply (19 V DC, 4.74 A) should be used.
However, is it possible to use a 12V DC power supply?
It seems good to input lower voltage than 19V according to the specification of input voltage for DLPA3005 and TPS54335A.
It would be helpful if you can give us any opinion for this question.
Thank you for your help.
Nobu Arai