Other Parts Discussed in Thread: DLPC3435, DLPA2005
Good-day,
We are using the DLP2010 chipset, (DLPC3435 and DLPA2005) in a small projector. What we are seeing is, on rare occasions, we get a white "bar" down the middle of the image from the projector. We removed the DMD from the projector and we could see a small line of mirrors that didn't appear to be parked correctly on power down. These mirrors appear to be stuck. Once in this condition we are not able to do anything that can reset them.
We were able to put the DMD under a microscope, and see the sections that were stuck. The three included pictures are all from the same device, and all the "voids" occur in the same 2-3 columns of the mirror array.
Is there any way to reset the mirror positions to remove these spots/lines?