This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010: Firmware update over I2C

Part Number: DLP2010
Other Parts Discussed in Thread: DLPA2000, DLPC3430,

Hi,

I have a system that consists of a a DLP2010 DMD, being driven by the DLPC3430, DLPA2000 chipset.  I'm looking to update the firmware and I was wondering if it is possible to perform the firmware update over the I2C connection to the DLPC3430. 

If so, is there any documentation available on how this can be done.?

Thank-you for your help. 

Kind Regards,


Stephen Craig
Design Engineer
Avalon Holographics
+1.709.765.6385
stephen.craig@avalonholographics.com