Other Parts Discussed in Thread: MSP430FR5969, MSP430WARE
Hello!
I have a DLP3010EVM-LC, and an MSP430FR5969 Launchpad. I am attempting to send commands to the DLPC via I2C using the J14 Connector; Per my requirements, I can't use/program the MSP430 onboard the Eval kit for anything, so it remains untouched.
I have it wired as follows:
J14 - Headers soldered on
Pin 1 - Connected to P1.6 (Pulled up to VCC via 10k resistor; tried with and without this)
Pin 2 - Connected to P1.7 (Pulled up to VCC via 10k resistor; tried with and without this)
Pin 3 - Connected to GND
Pin 4 - Connected to VCC
On the MSP430FR5969, I am using the EUSCI_B_I2C_* calls to send the commands. I copied the initialization code and most of the logic from MSP430Ware "Driver Library" examples in the Resource Explorer; however I am not using interrupts as some of the tx examples do.
It appears that the DLPC is not responding to any commands sent through this connector. When it is connected, the onboard buttons also do not respond (with and without pull-up resistors). I'm WFH Intern and working on getting a logic analyzer to check the I2C bus but at the moment I can't see why it isn't working.
Your guidance is appreciated, I can post more details as you need them. I'm pretty new to this world so I apologize if I use incorrect terms.