Part Number: DLPLCR9000EVM
Other Parts Discussed in Thread: DLPC900
Hi,
I'm asking for your help. I think I'll use a DLPLCR9000EVM.
I am interested in showing much more than 400 (which is the maximum number of loadable patterns) 1-bit patterns at the maximum speed possible.
So, I think I'm going to be forced to use the VIDEO PATTERN MODE.
On the "DLP® LightCrafter™ 6500 and 9000 Evaluation Module (EVM) User's Guide" I couldn't find any indications, but the
Table 2-85 on "DLPC900 Programmer's Guide Programmer's Guide" it says that the Maximum external input for video pattern mode is
2880 Hz for pattern 1-bit.
Does the DLPLCR9000EVM allow me to go up to 2880 Hz? Using which Interface (USB, HDMI, I2C or DP )?
If I used pre-loaded patterns, I would be forced to load 400 pattens (1-bit ) at a time, what would be the time needed to load them?
Thanks and regards,
Lorenzo