Part Number: DLP2010EVM-LC
I want to control 2D light patterns and exposures with this DLP.
I want to update patterns and synchronize with a camera using software. I do not need very high speed but hopefully I would like to achieve 10 Hz or so.
I read through the user guides and I guess the splash pattern mode is suitable for my purpose.
I understood the command in "3.7 Flash Update Commands" on "DLPC3470 and DLPC3478 Software Programmer's Guide"
but do not know the file format.
I would like to generate patterns with software like python and send it to the board.
Is there any sample code available that helps me understand?
Thanks.