Dear Madam or Sir,
i just repaired two Infocus IN83 an Benq W20000. The DMD-Chips are mounted as
shown in document: https://www.ti.com/lit/an/dlpa067a/dlpa067a.pdf
(#11 s.13).
There is shown a Thermal Pad (electrically insulating) between DMD-Chip and stud.
In the data sheet of the DLP9500 i can't find any information if the chips "Thermal
Interface Area" is electrically connected to signal ground.
In the Datasheet " DLP® Series-450 DMD and System Mounting Concepts ", site 20
says:
Be aware that the DMDs Thermal Interface area is electrically connected to signal ground
(through the Ceramic Carrier), and that some thermal pad materials are electrically conductive.
So i guess also on DMD9500 i have to use insulating thermal pads and can't use compound or
graphite pads.
I hope you can help to confirm my conclusion.
Thanks & Regards,
Ph. Pavsic