Hi,
Is possible to replace BeagleBone Black board by BeagleBone Ai board for DLP2000EVM?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is possible to replace BeagleBone Black board by BeagleBone Ai board for DLP2000EVM?
Thanks.
John,
The DLP2000EVM can interface with any host processor that is capable of RGB888 DPI video output. The AM572x on this device seems to support DPI output just like the standard BeagleBone Black's Sitara processor, so as long as you can configure the video output (and get I2C connection for sending commands to the EVM) you should be able to use this device the same as a BeagleBone Black.
That being said, the device drivers (cape overlay) won't be installed out of the box on this platform, so you may need to compile/load them yourself. There is some information about the cape overlay used with the DLP2000EVM (and a download link) here:
https://e2e.ti.com/support/dlp/f/94/t/663939
I hope this helps.
Regards,
Philippe Dollo