Part Number: DLPLCR9000EVM
I am a bit confused concerning the pattern rates. The programmers guide describes how a frame in video mode is displayed.
The minimal exposure time of single patterns is 105us and the bit depth for a single color is 8 so there are 255 intensity levels. How can this work with 60 fps? Having a bit depth of three and comparing a pixel with an intensity level of 255 with one of intensity level 1 means that the time interval of the 255 pixel has to be 255 times as large as the time interval of the 1 pixel. When I say that the short time interval is 105us than the long one would be 255*105 us = 26775 us which is 26.8 ms while 1/60s (60fps) gives 16ms. Where is my mistake?