Hello,
I have recently purchased DLPDLCR2000EVM + BeagleBone Black. As per the guidelines I have followed the steps (apart from installing debian, which was already installed). I can't see to be able to run the mplayer python file. It fails with
set slave address: 27 Make sure the display port is set. For example export DISPLAY=:0 1 SourceSel.EXTERNAL_VIDEO_PARALLEL_I_F_ 2 Resolution.NHD_LANDSCAPE ################################################################## play video nhd_test.mp4 MPlayer 1.3.0 (Debian), built with gcc-8 (C) 2000-2016 MPlayer Team do_connect: could not connect to socket connect: No such file or directory Failed to open LIRC support. You will not be able to use your remote control. Playing nhd_test.mp4. libavformat version 58.20.100 (external) Mismatching header version 58.12.100 libavformat file format detected. [mov,mp4,m4a,3gp,3g2,mj2 @ 0xb68b6348]Protocol name not provided, cannot determine if input is local or a network protocol, buffers and access patterns cannot be configured optimally without knowing the protocol [lavf] stream 0: video (h264), -vid 0 VIDEO: [H264] 640x360 24bpp 30.000 fps 3600.5 kbps (439.5 kbyte/s) vo: couldn't open the X11 display (:0)! vo: couldn't open the X11 display (:0)! vo: couldn't open the X11 display (:0)! vo: couldn't open the X11 display (:0)! VO XOverlay need a subdriver [VO_SDL] SDL initialization failed: Unable to open a console terminal. vo: couldn't open the X11 display (:0)! vo: couldn't open the X11 display (:0)! vo: couldn't open the X11 display (:0)! ========================================================================== Opening video decoder: [ffmpeg] FFmpeg's libavcodec codec family libavcodec version 58.35.100 (external) Mismatching header version 58.18.100 Selected video codec: [ffh264] vfm: ffmpeg (FFmpeg H.264) ========================================================================== Clip info: major_brand: mp42 minor_version: 1 compatible_brands: mp42avc1 creation_time: 2017-07-07T14:32:35.000000Z Load subtitles in ./ Audio: no sound Starting playback... Could not find matching colorspace - retrying with -vf scale... Opening video filter: [scale] Movie-Aspect is undefined - no prescaling applied. [swscaler @ 0xb6947400]bicubic scaler, from yuv420p to bgra using C [swscaler @ 0xb6947400]No accelerated colorspace conversion found from yuv420p to bgra. [swscaler @ 0xb6947400]using unscaled yuv420p -> bgra special converter VO: [fbdev] 640x360 => 640x360 BGRA [fs] Can't put VSCREENINFO: Invalid argument FATAL: Cannot initialize video driver. Movie-Aspect is undefined - no prescaling applied. [swscaler @ 0xb6947400]No accelerated colorspace conversion found from yuv420p to bgra.
Does anyone have any suggestions?
Many thanks