Hello,
For my application, I need to be able to display 10,000 binary patterns ~ @ 15 Hz according to the external TTL pulse that I input into the device. I know there is a limit to the number of patterns that can be loaded to the EVM at a time (400 for binary patterns). I have been trying to display these many patterns using the Pattern On-the-Fly Mode by creating multiple .txt files, each of which contains 400 patterns and loading them manually (all the patterns were pre-generated and stored in a folder). However, I have realized this approach is sub-optimal, generating a lot of errors in the measurement process.
Is there any recommended approach for displaying this many patterns? Should I use the video pattern mode or pattern on-the-fly mode with batch files? Please keep in mind that the patern display needs to be synched with an external trigger. Could you also give me step-by-step instructions for your recommended approach?
Thanks,
Daniel