Other Parts Discussed in Thread: DLP2010NIR, , DLPA2005, DLP2010
Hi,
We are developing a system using the DLP2010NIR. We designed our system based on the circuit diagrams provided for the evaluation module. Despite everything else seems to be correct, our DLPC150 chip cannot load the firmware successfully, i.e. we don't get the expected high to low transition on the HOST_IRQ pin, it remains high all the time.
Let me describe our current situation:
To make sure we programmed the flash IC correctly, we soldered it directly on the eval module, programmed it through the TI software, checked that it's working and transferred it to our circuit. DLPA2005 does produce all the correct voltages, PROJ_ON signal is high, DMD is connected, we have a 10k pull-up resistor on the HOST_IRQ pin, there seems to be some activity on the flash SPI lines so the chip is active. When we disconnect the DMD and power-up, DLPA2005 enters the standby mode: Voffset and Vbias = 4.5V, Vrst = 0.45V. When the DMD is connected we get the proper voltages, so the device can switch between Active1 and Standby modes.
Do you have any suggestions?
Thanks,
Kıvanç Hedili