Other Parts Discussed in Thread: DLP4500
Good Morning,
I need a few more details regarding the optomechanics of the DLP4710.
- what is the width of the gap between two TRP micromirrors? (in % of Pixel pitch or in mu)
- what are the values of the "Micromirror array fill factor" and of the "Mirror metal specular reflectivity"? (both values are provided for example for the DLP4500 (§7.10, p22)
- is the "Mirror metal specular reflectivity" the reflectivity of a single Micro Mirror or of the whole DLP array?
- can one assume that the reflectivity of a micromiror is identical in the middle and on the border of the Mirror? Or should we expect a loss of reflectivity along the micromirror border, resulting in an effectively increased gap?
Thanks in Advance for your information
regards
Matthieu